- Published 1 Feb 2024
- Last Modified 1 Feb 2024
- 8 min
A Comprehensive Guide to Air Quality Monitors & Sensors
Explore air quality monitor types, functions, and expert tips for how to choose one. Learn to monitor air effectively for safer and healthier environments.

Understanding Air Quality Monitors and Sensors
Air quality monitors, also known as air quality sensors or pollution sensors, are sophisticated devices engineered to assess and measure various pollutants and particulate matter present in the air surrounding us. Their primary role is to evaluate and provide information about the quality of the air we breathe.
These devices utilise specialised sensors that detect and quantify different types of pollutants and gases present in the atmosphere. They measure substances such as volatile organic compounds (VOCs), particulate matter (PM), carbon dioxide (CO2), carbon monoxide (CO), ozone (O3), nitrogen dioxide (NO2), and other harmful gases or particles.
Air quality monitors have diverse applications across various settings. They are used in industrial workplaces, construction sites, offices, homes, schools, and more. Professionals such as tradesmen, industrial workers, health and safety officers, and environmental consultants rely on these devices to ensure safe working conditions and to identify potential hazards posed by air pollutants.
Air quality monitors and sensors serve as essential tools in assessing and understanding the quality of the air we breathe. Their ability to detect pollutants and provide crucial data empowers individuals and professionals to take proactive measures to safeguard health and promote better living and working environments. In the rest of the article, we’ll cover more about these amazing devices.
The Technology Behind Air Quality Sensors
Air quality monitors operate using various sensor technologies to detect and quantify different pollutants and particulate matter present in the air. These sensors function based on specific principles tailored to detect diverse types of pollutants. There are several types of sensor technologies that are commonly used in air quality monitors that we’ve provided more detail on below:
- Electrochemical Sensors: These sensors function by measuring the electrical currents produced when a chemical reaction occurs between the target gas and an electrode. They are commonly used to detect gases like carbon monoxide (CO), ozone (O3), nitrogen dioxide (NO2), and sulphur dioxide (SO2). When the sensor reacts to the presence of specific gases it causes a change in electrical current which feeds back to the attached monitor.
- Optical Sensors: Utilising light absorption or scattering principles, optical sensors measure particulate matter concentrations in the air. The optical sensors emit light through the air and the scattering or absorption of this light provides information about the concentration of particulate matter to the monitor. They are proficient in detecting fine particles, which are detrimental to health.
- Metal Oxide Semiconductor Sensors (MOS): MOS sensors work by detecting changes in electrical conductivity when in contact with gases. They are sensitive to volatile organic compounds (VOCs), like benzene, xylene, or other organic compounds, and are used to measure indoor air quality. Their ability to change conductivity when exposed to certain gases, enables them to detect and quantify potential pollutants in the air.
Once the sensors detect pollutants, the monitor collects and processes this information. It may display real-time data or store it for later analysis, depending on the monitor's capabilities. Air quality monitors leverage specialised sensor technologies to detect and measure pollutants present in the air. Understanding how these sensors operate helps in comprehending the data they provide, enabling individuals and professionals to take appropriate actions to improve air quality.
Common Applications for Air Quality Monitors
Air quality monitors find extensive applications across various sectors and settings, playing a key role in ensuring a healthy and safe environment. In New Zealand, both indoor and outdoor air quality are regulated and must meet certain standards. Outdoor air quality is regulated under the <u>National Environmental Standards for Air Quality</u>, or NES-AQ, which sets out certain levels that must be maintained for different types of pollutants and particulate matter. Indoor air quality on the other hand is regulated in combination with ventilation under <u>NZS 4303:1990</u>.
Industrial Workplaces
Air quality monitors are crucial in industrial settings where exposure to hazardous chemicals, gases, and particulate matter is prevalent. They help in monitoring and mitigating workplace pollution levels, ensuring the safety and well-being of workers in these environments.
Construction Sites
Construction sites generate dust, fumes, and other airborne particles that can pose health risks. Air quality monitors aid in assessing the levels of pollutants, allowing for measures to reduce exposure and maintain a healthy and safe work environment.
Offices and Indoor Environments
Indoor air quality is essential for health and productivity. Monitors help in evaluating indoor air pollutants like VOCs, CO2, and other contaminants, enabling individuals to take steps to improve air quality by adjusting ventilation or eliminating sources of pollution.
Residential Spaces
Ensuring clean air in homes is crucial for the health of occupants. Air quality monitors assist in detecting indoor pollutants, helping residents take actions such as using air purifiers or minimising the use of certain chemicals to improve indoor air quality.
Environmental Monitoring
Monitoring outdoor air quality is vital for assessing pollution levels in the environment. Air quality monitors placed in urban areas, near traffic zones, or in proximity to industrial facilities help in tracking pollutants and evaluating their impact on public health and the ecosystem.
Health and Safety Assessments
These monitors are employed in health and safety assessments, aiding professionals in identifying potential health hazards due to exposure to airborne pollutants. They are used in healthcare facilities, laboratories, and research environments to ensure safe working conditions.
Air quality monitors serve diverse purposes, from safeguarding worker health in industrial settings to ensuring clean indoor air in homes and offices. Their applications span across various sectors, playing a crucial role in assessing, monitoring, and improving air quality in different environments.
Different Types of Air Quality Monitors
Indoor Air Quality Monitors
Tailored for enclosed spaces like homes, offices, schools, and healthcare facilities, these monitors measure levels of volatile organic compounds (VOCs), carbon dioxide (CO2), temperature, humidity, and other indoor air pollutants. They are crucial for ensuring healthy indoor environments by detecting pollutants affecting occupants' health and comfort.
Outdoor Air Quality Monitors
Designed for installation in outdoor environments such as urban areas or near industrial sites, these monitors track pollutants like particulate matter (PM2.5, PM10), nitrogen dioxide (NO2), sulphur dioxide (SO2), and ozone (O3) in the ambient air. They aid in assessing air quality in outdoor spaces and understanding the impact of pollutants on public health and the environment.
Fixed or Stationary Air Quality Monitors
Permanently installed in specific locations for continuous monitoring of air quality parameters, these monitors offer continuous data for long-term assessment and analysis. They play a crucial role in ongoing monitoring in critical areas like industrial sites, traffic zones, or areas prone to pollution.
Particulate Matter (PM) Monitors
Specifically designed to measure airborne particulate matter of various sizes (PM1, PM2.5, PM10), these monitors assess the concentration and types of particles present in the air. They are essential for evaluating health risks associated with inhaling fine particles and understanding their sources.
The array of air quality monitors available allows for versatility in monitoring different pollutants and environments. By choosing the right type of monitor, individuals and professionals can effectively assess and manage air quality in various settings, contributing to healthier and safer environments.
Choosing the Right Air Quality Monitor
Selecting an appropriate air quality monitor involves considering several crucial factors to ensure it aligns with specific needs and environmental conditions. When beginning your research, defining the intended purpose and the pollutants requiring monitoring is essential. Whether assessing indoor air quality, tracking outdoor pollution, detecting specific gases, or measuring particulate matter, understanding these requirements is pivotal. Next, build an understanding of the sensor technology and its accuracy. Different sensors, like electrochemical for gas detection or optical for particulate matter measurement, offer varying levels of precision.
Consider the monitor's data reporting capabilities, including real-time data, connectivity options, and data output compatibility with analysis systems. Assessing the initial cost, ongoing maintenance expenses, can also help when selecting the most suitable monitor. Taking all of this into account will help to ensure you choose the right air quality monitor for the job.
Frequently Asked Questions about Air Quality Monitors
Popular Air Quality Monitor and Sensor Brands
Renesas Electronics
Based out of Japan, Renesas Electronics provides a range of quality products and sensors available at RS.
Testo
Specialised in measuring equipment, Testo offers a wide range of sensors and monitors.
Related links
- Air Quality Monitors
- Schneider Electric SLPSTXX Air Quality Monitor for Air Quality +50°C Max, AC Adapter-Powered
- Siemens QPM2102 Air Quality Monitor for CO2, VOC
- Schneider Electric SLPWLXX Air Quality Monitor 95%RH Max, AC Adapter-Powered
- Schneider Electric SLABTXX Air Quality Monitor 95%RH Max, AC Adapter-Powered
- Schneider Electric SLPSTXX Air Quality Monitor for Air Flow +50°C Max AC Adapter-Powered
- Schneider Electric SLPWXXX Air Quality Monitor for Air Flow +50°C Max AC Adapter-Powered
- Schneider Electric SLPSLXX Air Quality Monitor for Air Flow +50°C Max AC Adapter-Powered