- Published 23 May 2024
- Last Modified 23 May 2024
- 5 min
Understanding TRIACs: A Comprehensive Guide
TRIACs are a useful tool for people building AC circuits, but how do they work and what are the main TRIAC applications?

How TRIACs Operate

TRIACs, a fundamental component in AC circuits, serve various functions. But what exactly are they, and how do they function? Let's delve into TRIACs' mechanism and explore their primary applications.
Exploring TRIAC Functionality
If you've ever adjusted the speed of an electric fan, dimmed a room's lights, or controlled a motor's operation, you've likely encountered TRIACs. These electronic devices facilitate power switching and control within AC circuits, offering versatility across a spectrum of applications.
Unveiling TRIACs

TRIACs, semiconductor devices composed of silicon, permit electron flow in both directions through three electrodes. Constructed with four layers of silicon, they exhibit a PNPN function in the positive direction and an NPNP function in the negative direction.
Understanding the Acronym: TRIAC
TRIAC, short for 'triode for alternating current,' is commonly classified alongside silicon-controlled rectifiers (SCRs) and thyristors. Noteworthy functions of TRIACs include:
- Amplifying power from low to medium voltage, akin to other triodes.
- Facilitating bidirectional flow of AC currents, in contrast to SCRs and thyristors.
- Featuring two distinct states: on and off, resembling other thyristors.
- Conducting triggered by gate signals, akin to an SCR.
Practical Applications
Given their unique characteristics, TRIACs find utility as both switches and power control units within AC circuits.
Navigating TRIAC Symbolism
The circuit symbol for TRIACs depicts the device's three electrodes, comprising both anodes and the gate. While variations may exist in TRIAC construction, all devices entail two SCRs linked antiparallel via a cathode and anode. Consequently, both terminals are designated as anodes, alongside a shared gate for the SCRs within the device.
Understanding TRIACs: Principles and Operation
Delving into TRIAC Operation
While often likened to two thyristors functioning in antiparallel, TRIACs boast a unique construction—featuring a blend of N-type and P-type areas—that enables them to execute switching functions across both segments of the AC waveform. This distinctive attribute grants TRIACs the ability to accommodate current flow in either direction, rendering them indispensable in a myriad of applications.
Bidirectional Conduction
Unlike conventional thyristors, TRIACs exhibit the capability to conduct irrespective of the polarity applied to their terminals. Consequently, a single TRIAC suffices for numerous applications, enhancing convenience and efficiency. However, it's essential to note that triggering the device demands varying levels of current sensitivity, with the highest threshold occurring when both terminals share the same polarity.
Exploring Triggering Modes
The operation of TRIACs encompasses four distinct triggering modes, each characterized by specific configurations:
I+ Mode:
In this mode, Terminal 2 current is positive, accompanied by positive gate current.
I- Mode:
Here, Terminal 2 current remains positive, while the gate current is negative.
III+ Mode:
Terminal 2 current assumes a negative polarity, while the gate current remains positive.
III- Mode:
In this mode, Terminal 2 current is negative, coinciding with negative gate current.
Understanding these triggering modes facilitates precise control and utilization of TRIAC devices across various applications.
Utilizing TRIACs: Applications and Testing
Exploring TRIAC Applications
The intrinsic requirement of a gate-triggering mechanism renders TRIACs an optimal choice for constructing switches in low-to-medium power AC circuits. This versatility extends to various functionalities, including light, fan, and motor controls, as well as integration into temperature and liquid level control systems.
TRIAC in Switch Circuits
To effectively employ TRIAC circuits for AC switching, the following sequence of actions is imperative:
- With the switch (SW1) open in the circuit, the TRIAC remains in the 'OFF' state, allowing no current to flow through the lamp.
- Upon closure of the switch, a trigger signal is conveyed to the TRIAC via the gate electrode, prompting the device to transition into its 'ON' phase.
- When solely AC power is provided to the TRIAC, the device undergoes unlatching and relatching during each half-waveform cycle. This facilitates controlled regulation of the current flowing through the lamp.
- The TRIAC ceases to conduct only when the supplied current diminishes close to zero.
Testing TRIACs
To assess the functionality of a TRIAC, a digital multimeter (DMM) proves indispensable. Ensuring the efficacy of the device entails the following steps:
- Connect the positive and negative leads of the DMM to each terminal of the TRIAC.
- The DMM should register an infinite resistance reading.
- Alternatively, employing a jumper wire to short-circuit the TRIAC gate should yield a resistance reading of 0.
- Reversing the leads on each terminal will revert the DMM reading back to infinity.
Obtaining these readings through systematic testing verifies the TRIAC's proper functionality within the circuit.
Popular Brands
Related links
- Unveiling the Essentials: A Comprehensive Guide to Isolators
- Solid State Relays: A Comprehensive Guide
- Understanding Continuity Testers: A Comprehensive Guide
- A Comprehensive Guide to Rheostats
- A Comprehensive Guide to Flow Switches: Types and Installation
- Wingnut Mastery: A Comprehensive Guide for Trades and Pros
- Mastering 3D Scanners: A Comprehensive Guide to 3D Scanners
- What is a Flow Meter?