Arduino M0 Pro development board now available at RS Components for innovative Internet of Things applications | RS

Press Releases


Arduino M0 Pro development board now available at RS Components for innovative Internet of Things applications

New board builds upon Arduino Uno platform with more processing capability via low-power 32-bit Atmel microcontroller based on ARM Cortex® M0+ core

New Zealand, 2 July 2015:

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has announced availability of the Arduino M0 Pro[1], a simple and powerful extension of the 32-bit Arduino platform established by the Arduino Uno board.

Aimed at embedded engineers, hackers and students, the new Arduino M0 Pro board is designed to help the development of innovative ideas for smart Internet-of-Things (IoT) devices, wearable technologies, high-tech automation, robotics and other imaginative projects. As well as enabling new project opportunities, the board is highly suitable as an educational tool for learning about 32-bit application development.

Fuelled by the low-power Atmel SAM D21 microcontroller, which integrates the 32-bit ARM Cortex® M0+ core, the Arduino M0 Pro board expands the Arduino family with increased performance and a highly flexible feature set. A key feature of the board is the Atmel Embedded Debugger (EDBG), which provides a full debug interface without the need for additional hardware and significantly increases ease-of-use for software debugging. The EDBG also supports a virtual COM port that can be used for device programming and traditional Arduino boot loader functionality.

Compatible with 3.3V shields that conform to the Arduino R3 Layout, development using the Arduino programming language is fully supported through a custom developed software library, integrated in the Arduino development environment.

Key hardware specifications of the M0 Pro board include: ATSAMD21G18 MCU running at 48MHz and packaged in a 48-pin LQFP, 3.3V operation, 256KB of Flash memory, 32KB of SRAM and EEPROM of up to 16KB via emulation. Input/output options include 14 digital I/O pins with 12 PWM channels and UART, six 12-bit ADC input channels and a 10-bit DAC output.

The Arduino M0 Pro development board is shipping now from RS Components.




[1] Formerly known as Arduino Zero Pro

About RS Components

RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping around 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2015 had revenues of £1.27bn.

For more information, please visit the website at www.rs-online.com.

Further information is available via these links:

Twitter: @RSElectronics; @alliedelec; @designsparkRS

RS Components on Linkedin
http://www.linkedin.com/company/rs-components

Relevant Links:

Electrocomponents plc
www.electrocomponents.com

RS Components
www.rs-online.com

DesignSpark
http://www.designspark.com