Press Releases
RS Components adds most productive 8-bit microcontrollers to embedded portfolio
Busy Bee, Sleepy Bee and Universal Bee series are perfectly adapted to solve extreme power, space and cost challenges
New Zealand, 2 July 2015:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, is now supporting all three Silicon Labs EFM8 microcontroller series based on the ubiquitous 8051 8-bit core, comprising a broad selection of devices that are ideal for highly focused, energy-conscious and space-efficient applications. Low-cost development kits for all devices are also in stock.
EFM8 Sleepy Bee devices are extremely energy friendly, running at a core speed of up to 25MHz and offering multiple power-management modes. The sleep current of 50nA is among the lowest of any microcontroller, and the active current of 150µA/MHz ensures thrifty performance in any battery-powered application. The peripherals, on the other hand, are empowering: 14 capacitive sense channels, 12-bit ADC, precision oscillator, low-current comparator and voltage reference. There are also four 16-bit timers, a UART, and support for I2C, SMBus and SPI.
The Busy Bee devices present a highly economical option. Two series are available, offering the choice of 25MHz or 50MHz maximum CPU speed, and the devices offer versatile peripherals including two analogue comparators, 12/10-bit SAR ADC, four 16-bit timers, plus I2C, SMBus and SPI.
For applications needing USB connectivity, the EFM8 Universal Bee microcontrollers add a crystal-less full-speed/low-speed USB2.0-compliant controller with 1KB buffer memory and clock recovery. There are also two UARTs and up to two I2C/SMBus ports. Universal Bee devices are offered in two series with up to 16KB or 64KB of on-chip Flash.
All EFM8 microcontrollers feature a priority crossbar encoder that allows small packages by managing pin assignments so as to eliminate conflicts. Busy Bee and Sleepy Bee microcontrollers are offered in packages as small as 3mm x 3mm QFN20, as well as hand-solderable 24-pin QSOP or 16-pin SOIC (Busy Bee 2). The Universal Bee devices are offered in packages from 3mm x 3mm QFN20 to hand-solderable 32-pin LQFP or 48-pin TQFP (Universal Bee 2).
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping around 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2015 had revenues of £1.27bn.
For more information, please visit the website at www.rs-online.com.
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com