- Published 23 May 2024
- Last Modified 23 May 2024
- 6 min
A Complete Guide to AC/DC Adapters
Read our AC/DC adapters guide to learn how they work and understand the adapter types, voltages, brands, and FAQs.

Introduction to AC/DC Adapters
Discover the ins and outs of AC/DC adapters, gaining insight into their functionality, various types, voltage specifications, top brands, and commonly asked questions (FAQs).

What Exactly is an AC/DC Adapter?
In New Zealand, AC/DC adapters serve as essential external power supply units for electrical devices that cannot directly access power from the mains network. These adapters play a crucial role in converting alternating current (AC) into the necessary direct current (DC).
Typically, electronic devices lack the internal space needed for the bulky components required for this conversion process. Hence, the use of swappable external power supply units offers increased flexibility and convenience.
While phone and laptop chargers represent the most recognizable form of AC/DC adapters, they serve a myriad of purposes in industrial settings. For instance, they find applications alongside motors and automation equipment.
AC/DC adapters go by various names, including:
- AC DC adapters
- AC/DC converters
- AC chargers
- DC adapters
- AC adapters
- AC adapter plugs
- Battery chargers
- Switching adapters
- Plug-in power supplies
- Power adapters
Explore our extensive range of AC/DC adapters tailored to meet diverse needs and requirements.
How Do AC/DC Adapters Work?

Understanding the Difference Between AC and DC Power
In New Zealand, it's essential to grasp the distinction between AC (alternating current) and DC (direct current) power formats. AC power oscillates, changing direction between positive and negative poles within a circuit. This dynamic format is utilized for delivering mains electricity. Conversely, DC power maintains a constant direction without oscillation. It's employed for transmitting electricity along electrical pylons and powering devices such as telecommunications equipment, vehicle batteries, and those equipped with rechargeable batteries.
The Inner Workings of AC Adapters
AC adapters typically consist of a compact central unit housing power-switching circuitry. This unit draws AC power from the mains and converts it into DC at the specific voltage required by the device. A power cord then channels this converted power from the adapter to the device, facilitating battery charging or operation.
Designed for Versatility and Compatibili
Like most electrical devices, AC adapters are engineered to be compatible with various power levels, typically measured in volts. Additionally, they come equipped with a range of plugs to accommodate different socket designs. For instance, the standard UK power plug differs from that used in Europe and the USA.
While many AC/DC adapters are tailored for specific devices, some models offer universal compatibility. These versatile power supply adapters can function as replacement chargers for a broad spectrum of devices. They support multiple voltages within a specified range, such as 100-240 volts, and may even feature interchangeable plugs of varying sizes, known as star connectors or X connectors.
AC/DC Adapter Types: Understanding the Varieties
Overview
AC/DC adapters are engineered to execute a straightforward task: powering direct current devices within an alternating current environment. Despite this simplicity, a plethora of configurations and specifications exist. Keep an eye out for variances in:
- Amperage levels
- Input and output voltages
- Plug types (both input and output connectors)
- Power ratings
- Approvals such as Medical/UL standards
- Surge/ESD protection
Additional Variations
Wall Mount vs. Desk Mount
Wall Mount Adapters: These adapters plug directly into a wall socket and connect to the recipient device via a cable.
Desk Mount Adapters: In contrast, desk mount adapters are positioned between the mains plug and the device, with cables extending to both. They are commonly employed with printers and similar devices not intended for portability.
Protection Against Overvoltage and Overcurrent
Surges in voltage and current pose a threat to equipment integrity and may even lead to fires. Incorporating circuitry designed to deactivate in response to power surges aids in minimizing this risk.
Short Circuit Protection
Short circuits occur when electrical resistance within a circuit drops, diverting current from its intended path and potentially causing damage or equipment failure. Short circuit protection mechanisms may include hardwired current limits or automatic resets triggered in response to overheating.
AC/DC Adapter Plug Types: Catering to International Standards
Globalization of AC/DC Adapters
In the era of global consumer technology, AC/DC adapters have become universal products. However, variations in wall socket designs across countries necessitate different plug types. For instance:
- British Plugs: Characterized by three conducting pins.
- American Plugs: Utilize a two-blade (flat pin) arrangement.
- Australian Plugs: Feature three blades.
- European Plugs: Comprise two cylindrical pins.
- Japanese Plugs: Favor dual blades with circular indentations.
Adapting to International Variations
Manufacturers tackle this issue in two primary ways:
- Regional Models: Producing adapters with integrated plugs tailored to specific regions.
- Interchangeable Charger Plates: Supplying adapters with a set of interchangeable charger plates featuring different regional plug designs. Users select and attach the appropriate plate for their country, allowing for cost-effective adaptability to a broader market.
Understanding AC vs. DC Adapters
While the terms AC and DC adapters are often used interchangeably, they emphasize different aspects:
- AC Adapter: Focuses on the use of mains power.
- DC Adapter: Highlights the converted charge used to power the device.
Though less common, AC adapter may also refer to electrical transformers that produce AC at a different voltage than the input.
Input and Output Voltages
Input Voltage:
The input voltage of an AC/DC adapter denotes the power level supplied to the adapter by the mains, standardized and varying across regions. For example:
- UK and EU: Standardize at 230V.
- US: Standardize at 120V.
An adapter with an input level of 100-240V is compatible with both standards. Additionally, the input voltage may include the Hertz (Hz) frequency rating, indicating the number of times per second the current changes direction.
Output Voltage:
Following conversion to direct current (DC), the adapter passes a lower level of charge to the device. Common output voltages include:
- 5V
- 9V
- 12V
- 15V
- 24V
- 48V (in select industrial applications)
The output voltage is typically quoted alongside the rated amperage, for instance, 12V 2A.
Frequently Asked Questions (FAQs)
Related links
- AC/DC Adapters
- RS PRO 20 W Power Adapter AC/DC Adapter 3-Pin (IEC) 5V dc Output, 4 A
- RS PRO 24 W Power Adapter AC/DC Adapter C14 6V dc Output, 4 A
- XP Power 90 W Power Adapter AC/DC Adapter 24V dc Output, 3.75 A
- RS PRO 72 W Power Adapter AC/DC Adapter C14 12V dc Output, 6 A
- RS PRO 36 W Power Adapter AC/DC Adapter C14 24V dc Output, 1.5 A
- Teltonika Power Adapter AC/DC Adapter Australia
- RS PRO 18 W Power Adapter AC/DC Adapter 3-Pin (IEC) 6V dc Output, 3 A