- Published 8 Feb 2024
- Last Modified 28 May 2025
- 10 min
Detecting Motion: Proximity Sensor Types and Applications
This guide explores the various types of proximity sensors available in New Zealand, including inductive, capacitive and ultrasonic sensors, and delves into their diverse applications across industries.

What are Proximity Sensors?
Proximity sensors, otherwise known as proximity detectors, are electrical components used to detect the absence or presence of an object within their vicinity without any physical contact. These sensors can use a range of different technologies, each suited to different applications, making them versatile tools in countless industries.
Corporates, Industrials, and everyday tradesmen often rely on these sensors for their precision and reliability in various tasks, from automating machinery to enhancing security systems. Proximity sensors come in a range of different types, employing distinct technologies to achieve their purpose, such as capacitive proximity sensors, inductive proximity sensors, or PIR (Passive Infrared) Sensors. While the technology used may be diverse their fundamental purpose remains the same, detecting proximity.
As we proceed through this article we’ll explore the different types of proximity sensors and their applications, providing you with the knowledge to use them effectively.
What is a Proximity Switch?
If you’ve just started looking into proximity sensors, you’ve likely come across proximity switches as well. What proximity switches are is a specific type of switch that contains proximity sensors. These devices function as binary switches, toggling between on and off states when an object enters or exits their sensing range. This makes them invaluable for a variety of uses in industrial and security settings.
How Does a Proximity Switch Operate?
A proximity switches’ function is to detect the presence of an object within a certain range without physical contact. How it operates is by emitting a field or beam (which can be magnetic, ultrasonic or electromagnetic, depending on what the sensor type is) and measuring changes in that field or beam caused by the presence of an object.
When an object enters the detection range, it alters the field or beam, triggering an internal switching mechanism within the sensor. This change in state is then translated into an electrical signal, which can be used for various purposes including controlling or automating processes.
The Different Types of Proximity Sensors and How They Work

Proximity sensors operate on different technologies, each with its own unique way of detecting objects within their vicinity. Understanding the working principles of these technologies is essential to making informed decisions on which type of proximity sensor is right for your specific application. These include:
Capacitive Proximity Sensors
Capacitive proximity sensors are used in industries like food processing, material handling and manufacturing where they can sense liquids, plastics and various other solid materials. Capacitive proximity sensors are not suitable for detecting ferrous materials, and typically work better for close range applications like level detection and monitoring.
Capacitive proximity sensors can be affected by environmental factors, and may experience interference from nearby objects or other sensors. This can include anything from ambient temperatures to other objects in their vicinity. Therefore, precautions must be taken when installing these sensors to ensure there is no interference with the sensor.
How Capacitive Proximity Sensors Work
Capacitive proximity sensors function by measuring changes in capacitance, which occur when an object enters their detection field. In simpler terms, the sensor contains a transmitter that generates an electric field. When an object disturbs the electric field, it triggers the sensor by affecting the capacitance of the two electrodes within the transmitter.
Inductive Proximity Sensors
Similarly to capacitive sensors, inductive proximity sensors can also be affected by their environment or the presence of other types of sensors in their vicinity. Inductive proximity sensors should be installed carefully to ensure that its performance is not affected by the surrounding environment.
How Inductive Proximity Sensors Work
Inductive proximity sensors utilise electromagnetic fields to detect metal objects. When a metal object enters the sensor’s range, it disrupts the electromagnetic field, leading to a change in inductance. This change triggers the sensor, making them valuable tools for detecting metal objects or ferrous materials.
Magnetic Proximity Sensor
Magnetic proximity sensors can typically operate at high speeds, making them effective tools for measuring high speed processes like rotational velocity. Due to their ability to only detect ferrous materials, they are more limited in their application, but are commonly used in industrial settings.
How Magnetic Proximity Sensors Work
Magnetic proximity sensors work by sensing changes in magnetic fields caused by the presence of a ferrous object. When the sensor detects a magnetic disturbance, it triggers an internal switching mechanism, which then activates the sensor's output, making these sensors suitable for applications like position sensing or door control.
Ultrasonic Proximity Sensor
Due to the way they function, ultrasonic proximity sensors can measure proximities over longer distances than other types of proximity sensors. Ultrasonic proximity sensors are typically used in applications such as obstacle detection and distance measurement.
How Ultrasonic Proximity Sensors Work
Ultrasonic proximity sensors emit high-frequency sound waves and then measure the time it takes for those waves to return after hitting an object. This is similar to how radar or sonar is used in navigation. By calculating the time delay, ultrasonic proximity sensors can determine the distance to an object and if there has been any change in its detection range.
PIR (Passive Infrared) Proximity Detection
Most PIR sensors have two sensing elements, and when one element detects a different level of radiation compared to the other it triggers the sensor. PIR sensors are particularly useful for detecting warm objects, such as people or animals, which is why they are often used in security applications.
How PIR (Passive Infrared) Proximity Detection Works
PIR sensors operate based on the fact that all objects with a temperature above zero emit infrared radiation. The word passive in the name PIR refers to the fact that these sensors do not emit any signal themselves, but instead simply observe infrared radiation levels. When an object moves within the sensor's field of view it causes a change in the amount of infrared radiation received by the sensor.
Dual Technology Proximity Sensors
Dual technology proximity sensors combine two or more sensing technologies to enhance accuracy and reliability. By requiring multiple detection criteria to be met, these sensors reduce the likelihood of false alarms compared to single-technology sensors. This makes them ideal for applications where accuracy and reliability are paramount, such as security systems and industrial automation.
How Dual Technology Proximity Sensors Work
More advanced proximity sensors make use of two or more technologies to provide enhanced detection capabilities. For instance, a sensor may combine ultrasonic and PIR sensor technologies to enhance accuracy and reliability in certain applications like occupancy detection in smart buildings. This combination allows for more robust detection, reducing the likelihood of false alarms or missed detections.
Proximity Sensor Applications
With their diverse range of technologies and capabilities, proximity sensors are used in a number of applications and scenarios. Their ability to detect objects without physical contact and trigger actions based on proximity makes them invaluable tools for enhancing efficiency, safety, and automation. In this section we’ll explore some of the key applications where proximity sensors play a pivotal role.
Manufacturing and Automation
Proximity sensors are extensively used in manufacturing and industrial automation. They can detect the presence and position of objects on conveyor belts, ensuring smooth production lines and providing additional safety in the case of something unintended ending up on the conveyor belt. These sensors can also play a critical role in ensuring quality by verifying the presence and alignment of components in the assembly process.
Security and Access Control
Security systems rely on proximity sensors, such as PIR sensors, for intrusion detection. Access control systems use these sensors to grant or deny access based on a person’s proximity or identification card and they are also employed in automatic door systems, where they can detect the approach of individuals and open the door accordingly.
Manufacturing and Automation
Proximity sensors are extensively used in manufacturing and industrial automation. They can detect the presence and position of objects on conveyor belts, ensuring smooth production lines and providing additional safety in the case of something unintended ending up on the conveyor belt. These sensors can also play a critical role in ensuring quality by verifying the presence and alignment of components in the assembly process.
Security and Access Control
Security systems rely on proximity sensors, such as PIR sensors, for intrusion detection. Access control systems use these sensors to grant or deny access based on a person’s proximity or identification card and they are also employed in automatic door systems, where they can detect the approach of individuals and open the door accordingly.
Automotive and Transportation
Proximity sensors, particularly ultrasonic sensors, are essential in the automotive industry. They are used for parking assistance, obstacle detection, and adaptive cruise control systems. In public transportation, these sensors are employed in automatic door opening systems and occupancy monitoring.
Consumer Electronics
Proximity sensors are increasingly common in consumer electronics. They are used in touchless interactions, such as automatic screen dimming or disabling touch input on your smartphone when it’s brought close to the face during a phone call. They also play a role in energy saving features by turning off screens when not in use.
Home Automation
In smart homes, proximity sensors are often integrated into a wide range of appliances and lighting fixtures. Proximity sensors can be used to detect when a person has entered or exited a room allowing for lighting to be turned on or off depending on the situation. They can also be placed around doors and windows to detect whether they are opened or closed, enhancing the security of the home. In combination with temperature sensors they can also work to adjust heating or cooling to enhance comfort and energy efficiency based on if people are detected in different areas of the home.
What to Consider When Selecting a Proximity Sensor
Selecting the right proximity sensor for a specific application is crucial to ensure optimal performance and efficiency. We’ll cover a few key considerations to keep in mind when selecting the right proximity sensor for the job.
Sensing Range: The sensing range of a proximity sensor is a critical factor. It determines how far the sensor can detect objects. Depending on the application, you’ll need to choose a sensor with an appropriate range to ensure it covers the required area effectively.
Material Detection: Take time to consider the type of materials the sensor will encounter. Capacitive proximity sensors are versatile for a wide range of materials while magnetic proximity sensors are only suitable for ferrous materials. Make sure the sensor you choose aligns with the materials present in your application.
Environmental Conditions: Evaluate the environmental conditions of the installation area. Factors such as temperature, humidity, and exposure to dust or liquids can impact proximity sensor performance. Ensure the selected sensor is rated for the environmental conditions it will be exposed to.
Output Type: Proximity Sensors can have various output types, including digital or analog signals, relay outputs, or even communication interfaces like RS-232 or RS-485. Choose the output type that integrates seamlessly with your control or automation system.
Compatibility: Ensure that the selected proximity sensor is compatible with your existing control system or microcontroller. This includes software compatibility and communication protocols.
By carefully considering these factors, you can make an informed decision when selecting a Proximity Sensor for your specific application. Whether you're a manufacturer or a tradesman, understanding these considerations is key to optimising processes, enhancing efficiency, and ensuring the success of your projects.
Frequently Asked Questions About Proximity Switches and Sensors
Popular Proximity Sensor Brands in New Zealand
Telemecanique Sensors
Experience seamless automation with Telemecanique Sensors’ reliable proximity sensors. Enhance your operations with quality and precision you can trust.
Related links
- Detecting Motion: Proximity Sensor Types and Applications
- A Guide to Electrical Relays: Types and Applications
- A Complete Guide to Load Cells
- Explained: How POE Injectors Power Networks & Devices
- Fused Spurs Buying Guide
- Springs: From Compressing to Helical, Types and Applications
- Magnetic Proximity Switches
- Proximity Sensors