New 3D Systems printers available from RS Components bring faster print speeds and higher resolution to consumers and professionals | RS

Press Releases


New 3D Systems printers available from RS Components bring faster print speeds and higher resolution to consumers and professionals

Cube® 3 and CubeProTM third generation 3D printers now available to pre-order from RS in Australia and New Zealand

New Zealand, 12 June 2014 :

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has expanded its 3D print offering with the introduction of the latest 3D printers from 3D Systems, a leading provider of 3D printing centric design-to-manufacturing solutions including 3D printers, print materials and cloud sourced on-demand custom parts for professionals and consumers. The new Cube® 3 and CubeProTM 3D printers are now available to order from RS in Australia and New Zealand, with delivery expected to start in July.

Cube 3 and CubePro offer multi-colour and multi-materials, ultra-high resolution settings of 70-micron thin print layers to give smoothness and fine detail, faster print speeds, and printing on-the-go from a smartphone app to be released by 3D Systems when product shipments begin. Both printers feature a colour touchscreen with an intuitive user interface and LEDs highlighting prints in action, and are equipped with fast Wi-Fi and Bluetooth connectivity.

Cube 3 is the only dual material, plug-and-play, child-safe IEC 60950 certified 3D printer that is easy to use. The printer is supplied with two starter cartridges in neon green and white, and 25 designs to start printing quickly. Cube 3 delivers up to two times faster print speed and accuracy than other printers on the market for printed parts up to 6” cubed. It prints in two materials and up to two colours, simultaneously using compostable PLA and recyclable ABS plastics. Both materials are available in 23 different colour cartridges. Instant material loading makes it easier than changing an ink cartridge. The new non-clog technology and moisture-lock cartridges ensure long shelf life and total material usage, improving print quality and sustainability.

The professionally capable CubePro is the only triple material, controlled print chamber engineer’s desktop 3D printer. It prints 2.5 times larger than any other desktop prosumer and hobbyist printer (10.8” x 10.45” x 9.5” or 275 mm x 265 mm x 240 mm), and guarantees faster, more precise prints with easy feed cartridges for prolonged material life. In addition to ABS and PLA plastic, CubePro also supports a new engineering grade nylon material, perfect for end-use applications.

Cube is a registered trademark of 3D Systems Corporation. CubePro is a trademark of 3D Systems Corporation.

About RS Components

RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer around 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping more than 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include semiconductors, interconnect, passives and electromechanical, automation and control, electrical, test and measurement, tools and consumables.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2014 had revenues of £1.27bn.

For more information, please visit the website at //www.rs-online.com

Further information is available via these links:

Twitter: @RSElectronics; @alliedelec; @designsparkRS

RS Components on Linkedin
http://www.linkedin.com/company/rs-components

Relevant Links:

Electrocomponents plc
www.electrocomponents.com

RS Components
www.rs-online.com

DesignSpark
http://www.designspark.com