Press Releases
RS Components introduces highly integrated CMOS-based differential air pressure sensors from Sensirion for building automation applications
Stable, highly accurate differential pressure sensors, based on innovative CMOSens® technology, target heating, ventilation and air-conditioning (HVAC) systems
New Zealand, 8 May 2017:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has announced availability of the SPD800 series of CMOS technology digital and analogue differential pressure sensors from Sensirion. Targeting high-volume applications, the sensors have been designed to measure the pressure of air and non-aggressive gases and deliver accurate and stable results covering a range of up to +/–500 Pa (+/– 5 millibars or +/– 2 inches of water), even at very low differential pressures.
The new sensor products are based on Sensirion’s innovative CMOSens® technology, which integrates a sensor element and all the necessary signal conditioning electronics – including analogue and digital signal processing – on a single tiny CMOS chip. The technology is well proven and is perfectly suited for high-quality and cost-sensitive volume production.
The SDP800 series sensor element, which uses flow-through technology to measure differential pressure, together with the on-chip signal processing and digital calibration, delivers high accuracy with no offset drift, right down to the lower end of the measurement range. These new CMOSens-based sensors largely overcome the limitations in offset drift and accuracy of traditional static or dynamic differential pressure sensors commonly used in HVAC applications. In conjunction with low-cost advantages, this makes them an attractive alternative for measuring differential pressure and airflow volumes in modern HVAC systems.
Available in the SDP800 series are the 4-pin +/–500 Pa SDP800-500PA, and the 4-pin +/– 125Pa SDP800-125PA. As well as offering characteristics including high reliability, long-term stability and an excellent signal-to-noise ratio, the sensors also feature a two-wire digital interface for easy connection to microcontrollers. In addition, the Sensirion EK-P5 evaluation kit enables easy and fast sensor evaluation via PC test software, connected via USB cable.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping more than 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2016 had revenues of £1.29bn.
For more information, please visit the website at www.rs-online.com.
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
RS WeChat ID: RS_Components_CN
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com