RS Components introduces new industrial I/O module, expanding capability of IOT2020 gateway for IoT applications | RS New Zealand

Press Releases


RS Components introduces new industrial I/O module, expanding capability of IOT2020 gateway for IoT applications

New SIMATIC IOT2000 is Arduino compatible and enables connection of non-critical sensor data

New Zealand, 21 June 2017:

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, today announced availability of the new SIMATIC IOT2000 module from Siemens, which is an Arduino-compatible shield that enables additional digital and analogue input/output (I/O) connectivity in an industrial environment. Designed to be compatible with the SIMATIC IOT2020 and IOT2040 industrial IoT gateways, the new module can be connected directly to local sensors to trigger non-time-critical processes.

Addressable via general-purpose I/O and programmable via high-level languages, the rugged IOT2000 module, or shield, is CE and UL certified and designed for 24/7 industrial operation. The range of I/O available includes five 24V digital inputs and two outputs, and two selectable analogue inputs, which offer 9-bit resolution and range from 0 to 10V or 0 to 20mA.

Originally launched in late 2016, RS is the sole authorised distributor for the open and flexible SIMATIC IOT2020 industrial IoT gateway, which is an Arduino-compatible device manufactured by Siemens. RS also recently signed a contract with Arduino that enables the IOT2020 to be marketed via the Arduino.cc shop and other sources to students, makers, geeks and young engineers, which is the primary target audience for Arduino.

The IOT2020 is extremely well suited for educational purposes and meets the many requirements of schools and universities to provide students with a platform to gain rapid experience of practical development, as well as enabling start-ups and makers to develop ideas in an open way into professional applications and projects. Offering a variety of interfaces such as Ethernet, USB and micro SD, the product is compatible with open-source software including the Arduino IDE and Yocto Linux, and can be programmed using high-level languages such as Java, C++ and JSON.

Heiko Luckhaupt, Industry Sector Marketing Manager at RS, commented: “The availability of the new SIMATIC IOT2000 module brings additional capability to the IOT2020, which is helping to bridge the gap between the Arduino-based electronic prototyping environment and world of industrial automation.”

About RS Components

RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping around 50,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2017 had revenues of £1.51bn.

For more information, please visit the website at www.rs-online.com.

Further information is available via these links:

Twitter: @RSElectronics; @alliedelec; @designsparkRS

RS Components on Linkedin
http://www.linkedin.com/company/rs-components

RS WeChat ID: RS_Components_CN

Relevant Links:

Electrocomponents plc
www.electrocomponents.com

RS Components
www.rs-online.com

DesignSpark
http://www.designspark.com